Working with the Topics List

The Topics List is MQTT-specific—it is only available on systems on which the MQTT driver is installed. Use the Display Topics pick action to display the Topics List for a particular MQTT Broker item in the database. The List contains entries for the topics that are associated with that particular broker.

As with other Lists, the Topics List consists of rows and columns. Each row represents an individual topic entry, and each column contains information about a specific value associated with that topic.

The Topics List contains these column headings:

As with other Lists, you can right-click on an entry in the List to display a context-sensitive menu (see Work with Common List Options).

Further Information

Display Topics pick action.


Disclaimer

Geo SCADA Expert 2020