Define the Button Font Settings for a Mimic

You can use the Text Font tab of the Mimic Properties window to define the default settings for the style, size and orientation of the lettering in buttons that you add to Mimics. This is useful when you know that you need to add multiple buttons to a Mimic, each with the same style of lettering. Rather than configure the font settings for each button separately, you can define the default font settings for buttons. After doing this, each button that you add will already have the default font settings in place. You can make further adjustments to each button by configuring its own settings separately if required.

Depending on the method that you use to display the Mimic Properties window, the settings you define will be applied to:

When you have displayed the Mimic Properties window using the appropriate method for your needs, define the Button Font settings as required. The various Button Font settings work in the same way as the similarly named settings on the Font tab of the Button Properties window (see Editing a Button).


Disclaimer

Geo SCADA Expert 2020