Define the Script Settings for a Mimic
You can use the Mimic Properties window to enable client-side scripting for a Mimic and also to access the Script Editor which you can use to create a Mimic script. The Mimic Properties script settings are:
- Enabled—Select the Enabled check box to toggle the scripting feature on and off for the Mimic. By default, the Enabled check box is clear (scripting is off).
- Edit—When you select the Enabled check box, the Edit button becomes available. When you select the Edit button, the Script Editor is displayed. You can use the Script Editor to create a script for the Mimic (see Display the Script Editor for a Mimic in the Geo SCADA Expert Guide to Scripting).
The Script settings are only available when you display the Mimic Properties window for an individual Mimic (rather than via the Options window).
For more information, please see Mimic Scripts in the Geo SCADA Expert Guide to Scripting.