Keyboard Shortcuts
You can use the following keyboard shortcuts when designing a Mimic:
Hold an Alt key when moving, resizing, or adding an object to disable the snap to grid feature. (Design mode).
- Hold a Shift key when adding an object to force a 1:1 size ratio.
- Hold a Shift key when adding a straight line to force an angle of 15°.
- Hold a Shift key when resizing to maintain the current aspect ratio.
Select the next object in order.
Nudge object left.
Nudge object right.
Nudge object up.
Nudge object down.
Hold a Ctrl key when you need to select multiple objects. Keep the Ctrl key pressed down as you select the objects in turn.
Toggle the grid on and off.
Make Group.
Break Group.
Toggle Run/Design Mode.
Bring Forward.
Send Backward.
Bring to Front.
Send to Back.
Next Layer.
Previous Layer.
The standard Windows keyboard shortcuts such as Ctrl+C for copy are also available.