Size Animations

There are 4 size properties that you can animate so that an object increases or decreases in size according to the value of an item in the database. This is useful for adding bar graphs to Mimics.

The size properties are:

Number for Expression Size Direction

0

None

1

Vertical down

2

Vertical center

3

Vertical up

4

Horizontal left to right

5

Horizontal left to right and vertical down

6

Horizontal left to right and vertical center

7

Horizontal left to right and vertical up

8

Horizontal center

9

Horizontal center and vertical down

10

Horizontal center and vertical center

11

Horizontal center and vertical up

12

Horizontal right to left

13

Horizontal right to left and vertical down

14

Horizontal right to left and vertical center

15

Horizontal right to left and vertical up


Disclaimer

Geo SCADA Expert 2020