Zoom Selection
You can use Zoom Selection to magnify a Mimic. The main advantage of the Zoom Selection over the other Zoom tools is that it allows you to specify which part of a Mimic is to be shown at an increased level of magnification.
To use Zoom Selection:
- Activate Zoom Selection:
In ViewX, select the Zoom Selection command
in the Navigation group on the Home tab.
In Virtual ViewX, right-click on the background of the Mimic to display a context sensitive menu, then select the Zoom Box option.
- Draw a selection box over the area that you want to magnify.
The area will be magnified when you release the left-hand mouse button. - Repeat this procedure as required.