Clearing an SMS Command Processor Excessive Failures Alarm

If the Fail Count for an SMS Service exceeds the Incoming SMS Fail Limit for the service, an alarm is raised. The alarm has a description that includes:

'SMS Command Processing suspended due to repeated failure(s) to process incoming SMS command(s)'.

To clear the alarm, you need to reset the Fail Count manually. For more information, see Resetting the Fail Count for Incoming SMS Commands.


Disclaimer

Geo SCADA Expert 2020