Diagnostic Battery Level

Associated with: SCADAPack 50 Outstations.

This status attribute is the SCADAPack 50 device's battery voltage level as last reported by the device.

For more information about monitoring the device's battery level, see Monitoring the SCADAPack 50 Device Battery Level.

NOTE: This attribute indicates the latest value that the device has sent to Geo SCADA Expert. The device transmits the data to Geo SCADA Expert in diagnostic SMS messages.


Disclaimer

Geo SCADA Expert 2020