Uncorrected Flow Volume
Associated with: Flow runs
This attribute indicates the total uncorrected gas flow volume that the Flow Run has calculated for the period. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller, if that Flow Run performs AGA-7 Flow Calculations. The units that apply to the attribute depend on the Measurement Units system being used for the Flow Run’s Contract Units.
Example:
353.2