Specify the Alert Notification Requirements
The SCADAPack x70 tab on the Forms of SCADAPack x70 Counter Configuration items contains an Alert Notifications section. Use the section to specify whether the SCADAPack x70 device is to store and report events and/or alerts (alarms) for the item.
The properties only apply when using a communications protocol that supports, and is configured to enable, event generation.
                 
            
The section contains the following property:
- Event/Alert Inhibit Enabled—Select the check box if the SCADAPack x70 device is to generate, store and report events and alerts (alarms) for the item.Clear the check box if the SCADAPack x70 device is not to generate, store or report events and alerts (alarms) for the item. This is the default setting.