Determine the Sub-Clause Types

When the Query Processor has created a list of the sub-clauses in your query, it begins to categorize the sub-queries according to type. By categorizing the sub-queries, the Query Processor can perform the remaining phases of the optimization algorithm more efficiently.

There are five categories of sub-clause:

When the Query Processor has categorized the sub-clauses, it places some of the sub-clauses in internal lists and some in the filter condition for the tables that are referenced. It uses the internal lists and filter conditions in a later phase of the algorithm. For example, the Query Processor places the access sub-clauses in an internal list so that when it needs to check the access sub-clauses for later phases of the algorithm, it can find the access sub-clauses quickly and efficiently.

When the Query Processor has categorized the sub-queries, it will proceed with the next phase of the SQL Optimization algorithm: Calculate the Table Order Permutations.


Disclaimer

Geo SCADA Expert 2020