Expressions.expr-primary-odbc-timestampadd
Adds a number of specified intervals to a timestamp
Format
{{ FN TIMESTAMPADD( IntervalType, Intervals, Timestamp ) }}
Remarks
Returns a timestamp calculated by adding a number of Intervals of IntervalType to Timestamp. Where Intervals can be any whole number numeric expression and Timestamp is any date\time expression.
The following table specifies possible values for IntervalType.
| IntervalType | Description |
|---|---|
| SQL_TSI_FRAC_SECOND | Thousandths of a second |
| SQL_TSI_SECOND | Seconds |
| SQL_TSI_MINUTE | Minutes |
| SQL_TSI_HOUR | Hours |
| SQL_TSI_DAY | Days |
| SQL_TSI_WEEK | Weeks |
| SQL_TSI_MONTH | Months |
| SQL_TSI_QUARTER | Quarters of year |
| SQL_TSI_YEAR | Years |
{ FN TIMESTAMPADD( SQL_TSI_SECOND, 15, TIMESTAMP '2006-08-02 00:00:00' ) }