App.LogOnUser and App.LogOffUser
The LogOnUser and LogOff functions are application functions and are used to log on/log off a specified system using a specified user name and password.
Syntax |
App.LogOnUser (System, User, Password) App.LogOffUser (System) |
Description |
The LogOnUser application function logs on to a specified system using a specified username and password. Unlike the LogOn application function, it does not display the Log On window or prompt the user to enter log on details. The LogOffUser application function logs off the specified system. Unlike the LogOff application function, it does not display the Log Off window or provide the user with the opportunity to cancel the log off request. |
Arguments |
System {String} The name of the system to which the specified user is going to be logged on/off. User {String} The user name that is used to log on to the specified system. Password {String} The password for the user name that is used to log on to the specified system. |
Returns |
None. |
Example:
App.LogOnUser ("SP1-SYS", "AYOUNG", "AY07AV")
This would log on to the SP1-SYS system via the AYOUNG user account using the password AY07AV.
Further Information