EditBox.VScroll

The EditBox Control Object that is returned by the AddEditBox function has a VScroll property. The VScroll property determines whether the Edit Box has a vertical scroll bar.

Syntax

ControlObject.VScroll = Value

Where ControlObject. is the name of the variable (declared in your script) that is used to store the EditBox Control Object that is returned by the AddEditBox function.

Description

Sets the vertical scroll bar for the Edit Box.

The scroll bar is are only visible if the Edit Box is set to have multiple lines.

Arguments

Value {Boolean}

If set to True (1), the Edit box has a vertical scroll bar; if set to False (0) it does not have a vertical scroll bar.

Returns

Boolean

Example:

EditBox1.VScroll = True

Where:

  • EditBox1 is the name of the variable that stores the EditBox Control Object returned by the AddEditBox function
  • True sets the Edit Box to have a vertical scroll bar.


Disclaimer

Geo SCADA Expert 2020