Form and Control Object Functions and Properties

The Form script object has functions and properties that allow you to create a Form and add various components to it such as fields, combo boxes, check boxes and so on. The Form functions that add settings to Forms return a special Form object called a ControlObject. Each ControlObject that is returned represents a specific setting and has common ControlObject properties as well as functions and properties that are specific to the type of setting that has been added. For example, Form.AddStaticText returns a ControlObject that has the common ControlObject properties as well as the StaticText properties.

The Form object and the ControlObject returned by some of its functions are available for use in both Mimic and Alarm Banner scripts. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2020