Mimic.SystemName
The Mimic.SystemName property returns the system name associated with the host of the Mimic script.
Syntax |
Mimic.SystemName |
Description |
Returns the system name of the system on which the Mimic that contains the script is running. |
Arguments |
None. |
Returns |
String |
Example:
MsgBox "Mimic System = " + Mimic.SystemName
This returns the name of the system and displays it in a message box.
The SystemName property is read-only.