PushButton.Text

The PushButton Control Object that is returned by the AddPushButton function has a Text property. The Text property represents the text that is shown on the button.

Syntax

ControlObject.Text = Text

Where ControlObject. is the name of the variable (declared in your script) that is used to store the PushButton Control Object that is returned by the AddPushButton function.

Description

Sets the string that is shown on the Push Button.

Arguments

Text {string}

Returns

String

Example:

PushButton1.Text = "Clear Form"

Where:

  • PushButton1 is the name of the variable that stores the PushButton Control Object returned by the AddPushButton function
  • "Clear Form" is the string that is shown on the button.


Disclaimer

Geo SCADA Expert 2020