Script Libraries

Script libraries are scripts that are stored in accessible items in the database. They can be referenced by any Mimic or Alarm Banner script and are designed to reduce the amount of time and effort required to create scripts that contain the same code. For example, if you create a Script Library that provides access to a Change Password Window, you can reference the Script Library from multiple Mimic scripts—the Mimics that reference the Script Library will be able to use the Change Password script, but do not need to contain the code of the Change Password script. This means that the amount of coding required for the Mimic scripts is significantly reduced as the code for the Change Password script only ever needs to be entered once (in the Script Library).

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2020