Server.RootObject

The RootObject property is a server property that represents the top level item in the database.

Syntax

Server.RootObject

Description

Represents the top level of the database (the Root of the database).

Arguments

None.

Returns

ServerObject

A ServerObject is a Geo SCADA Expert specific script object that has its own functions (see ServerObject Functions ) and properties (see ServerObject Properties) which can be manipulated.

Example:

The following script is used to display a message box that contains the name of the root object:

Set ServerRoot = Server.RootObject

MsgBox ServerRoot.Name

Where:

  • ServerRoot is the name of the variable used to store the ServerObject that is returned by the RootObject property.
  • MsgBox ServerRoot.Name instructs the script to display a message box that contains the Name value of the ServerObject that is stored by the ServerRoot variable (this is the ServerObject that is returned by the RootObject property).

Disclaimer

Geo SCADA Expert 2020