Server.SetOPCValue
The SetOPCValue function is a server function that allows a script to write a value to the database.
| Syntax |
Server.SetOPCValue (Tag, Value) |
| Description |
The SetOPCValue server function allows a script to write a value to an object property referenced by tag. |
| Arguments |
Tag {string} Defines the location of the database item to which the value is being written. Value {variant} The value defines the value that is written to the database. |
| Returns |
None. |
Example:
sDesc = InputBox ("Enter the New High High Desc")
Server.SetOPCValue ".AI1.HighHighDesc", sDesc
Where:
- sDesc = InputBox ("Enter the New High High Desc") instructs the script to display an Input Box that has the message "Enter the New High High Desc". sDesc is the name of the variable that is used to store the value that is entered in the input box.
- Server.SetOPCValue ".AI1.HighHighDesc", sDesc instructs the script to write the value that is stored in the sDesc variable (entered in the input field by the user) to the HighHighDesc configuration field of the 'AI1' point.