ServerQuery.ErrorMessage
The ServerQuery.ErrorMessage property provides a brief description of the cause of a failed SQL Query for the Server.Query.
Syntax |
ServerQuery.ErrorMessage |
Description |
Describes the cause of a failed SQL Query for the Server.Query property (see Server.Query). Typically, SQL error messages are due to the syntax of the SQL Query being incorrect. |
Arguments |
None. |
Returns |
Message {String}. |
For an example that shows how the ServerQuery.ErrorMessage property can be used, please refer to Server.Query.
Further Information
Constructing SQL Queries: see SQL Query Structure in the Geo SCADA Expert Guide to Lists.