ServerQuery.Rows

The ServerQuery.Rows property returns the values contained in the rows that are returned for the Server.Query property.

Syntax

ServerQuery.Rows

Description

Returns the values of the rows in the SQL Query that is returned by the Server.Query property (see Server.Query).

Arguments

None.

Returns

Rows {2 dimensional array of variants}.

The values of the rows in the Query that is returned by the Server.Query property.

For an example that shows how the ServerQuery.Rows property can be used, please refer to Server.Query.


Disclaimer

Geo SCADA Expert 2020