Clear Registry

Associated with: Users

Security permission required to access this pick action: System Admin

Use the Clear Registry pick action to clear the registry settings that are associated with a User Account. This includes values that are stored in the Geo SCADA Expert User Registry. This comprises name/value pairs that are used for Mimic animation, which are stored as part of the Geo SCADA Expert User Account (these are not entries in the Windows Registry). The pick action is only available if custom registry settings exist for the User Account (for example, due to the user using the SetRegistry or GetRegistry functions, or the REGISTRY method).


Disclaimer

Geo SCADA Expert 2020