Display the Users List

You can use the Users List to view information about the user accounts on your system.

The Users List can be filtered so that it only provides information about users with specific attributes.

To display the Users List:

In ViewX:

  1. Display the Queries Bar (see Display an Explorer Bar).
  2. Expand the Root Group (System icon) in the Queries Bar.
  3. Expand the System Queries branch.
  4. Double-click on the Users icon.
    The Filter Columns window is displayed.
  5. Use the Filter Columns window to apply any filtering as required (for more information, see Filter a List in the Geo SCADA Expert Guide to Lists).
  6. Select the OK button to confirm the filter selection.
    The Queries List is displayed.

In Virtual ViewX:

  1. Log on to Virtual ViewX.
  2. Select the Lists button to display the Lists page.
  3. Select the Users hyperlink.
    The Filter Columns window is displayed.
  4. Use the Filter Columns window to apply any filtering as required (for more information, see Filter a List in the Geo SCADA Expert Guide to Lists).
  5. Select the OK button to confirm the filter selection.
    The Queries List is displayed.

Alternatively, log on to ViewX or Virtual ViewX and select a link to the Users List from an appropriately configured Mimic.

Further Information

For other ways of displaying a List, see Display a List in the Geo SCADA Expert Guide to Lists.


Disclaimer

Geo SCADA Expert 2020