The Guest user account is a
Geo SCADA Expert has a single built-in User Group named Everyone. Every user account that is created is automatically associated with the 'Everyone' User Group
The Guest user account and Everyone user group should not be used. Instead, you should add 'configured' User Accounts and User Groups to the system and grant them the relevant security access and privileges. This provides greater flexibility and control over the functionality and features to which individual users, or groups of users, have access.
Some third-party applications such as OPC clients that do not support 'OPC Private Security' will need to use the Guest user to access Geo SCADA Expert. They require the Guest user account to have at least the Read permission so that they can access system data. This permission can be applied just to the objects which the application needs to read.
The Guest user account is not available on Virtual ViewX clients.