User Accounts Created from User Patterns

A User Pattern is a special type of user account. It defines the settings for new User accounts that are created automatically as part of an External Authentication process.

User Patterns only apply to systems on which Geo SCADA Expert user accounts and user groups are managed centrally outside of Geo SCADA Expert, by being integrated with corresponding Active Directory (AD) or Lightweight Directory Access Protocol (LDAP) user accounts and groups (see Integrate Geo SCADA Expert User Accounts with Active Directory or LDAP User Accounts).

If your system uses such a setup, when a new user attempts to log on to Geo SCADA Expert via ViewX or Virtual ViewX using user credentials for a user that exists in Windows or LDAP, but not in Geo SCADA Expert, a new user account will be added to Geo SCADA Expert automatically. In doing so, Geo SCADA Expert applies settings from the relevant User Group and User Pattern when creating the new User account. These settings determine the Geo SCADA Expert features to which the new user has access, the security permissions to which the user is assigned in Geo SCADA Expert, and so on.


Disclaimer

Geo SCADA Expert 2020