Back up the Server's Registry Settings

The topics in this section explain how to make a backup of your database at any time, typically for restoration or archival purposes. Geo SCADA Expert also has the ability to generate an automatic backup of the database whenever you upgrade the Geo SCADA Expert software on a server. This is a different type of backup. For more information, see Automatic Database Backup on Upgrade.

When you make a scheduled or on-demand backup of your database, we recommend that you include the server settings that are stored in one or more registry keys. The registry keys contain information about the server’s set up and are needed to help avoid configuration mis-matches if your backup files are loaded on to another server.

To include the Geo SCADA Expert registry keys in a backup, select the Registry check box on the Backup form (see Configure a Backup Database Item).

The registry files that you include in a backup can be restored by experienced system administrators if:

Geo SCADA Expert stores username and password information in the registry for use with features such as:

Such information is encrypted using machine details to prevent the encrypted data from being imported onto other machines. Encrypted data is intended only to be decrypted by the server that encrypted the data (and performed the backup). A diagnostic message is displayed if you attempt to restore encrypted registry settings on a different server:

This means that backing up the registry and then re-applying it to another machine requires you to recreate the security data, username, password and/or domain, in order to use the affected functions.

This is also true if Windows® is re-installed on the machine on which the data was encrypted.

ATTENTION: Reloading of backup files should only be performed by experienced system administrators. Please seek advice from Schneider Electric if you are unsure about restoring a backup (see Load your Backup Database Files). Loading backup files such as registry settings without expert guidance could have an unexpected effect on your system and could even stop a Geo SCADA Expert server from running.


Disclaimer

Geo SCADA Expert 2020