Choose the Database Table for an Extra Field

Each custom field is added to a table in the database. The table to which you add an extra field affects where the custom field is shown. For example, if you add a field to the CDBPoint table, the custom field will be shown on Point Forms.

To define the database table for an extra field, you need to use the Edit Field window (see Add or Modify an Extra Field).

When you have displayed the Edit Field window, you can define which database table will contain the field by using the Table setting:

When you have defined the Table, you can continue to define the other field settings as required.


Disclaimer

Geo SCADA Expert 2020