Mimics can contain animated representations of a channel. The Mimic can be configured to indicate the channel's log status as a background color. If logging is enabled on the channel, the background is dark yellow/mustard (default settings).
                 
            
If logging is disabled on the channel, the background color is white (default settings).
The change of color is a visual indication of logging being enabled. This can act as a reminder that logging needs to be disabled (it should only be enabled when you need to monitor communications).
To access a Mimic that contains an animated representation of a channel, you can:
Either:
- Use the Database Bar to locate the Mimic.
- Right-click on the Mimic's entry.
 A context-sensitive menu is displayed.
- Select the Display Mimic option.
 The Mimic is displayed.
Or:
- Select a hyperlink to the required Mimic (if a hyperlink has been configured).