Communications State - Failed: Invalid Host

A channel can fail due to the server being unable to obtain the IP address of the remote computer.

We recommend that you:

  1. Check that the Node Name that is defined in the configuration of the remote serial channel matches the name of the remote computer.
  2. Check the network setup and equipment.
  3. Check the network connection by 'pinging' the remote computer from the main server. To do this, access the Microsoft Windows Command Prompt and enter:
  4. Ping <name of remote computer>

  5. Do not enter the angle brackets.
  6. If the network connection is working correctly, the remote computer server will return data that you will see in the Command Prompt window. If there is no reply, there is a fault with your network.

Disclaimer

Geo SCADA Expert 2020