Create a Blank Database

When you have installed Geo SCADA Expert and configured the settings for the server(s), you need to create a blank database.

To create a blank database:

  1. Right-click on the Geo SCADA Expert Server icon.
    A context sensitive menu is displayed.
  2. Select the Start Database option.
    A dialog box is displayed.

  3. Select the Start Database button to create a blank database.

    ATTENTION: If this is not the first time that you have installed Geo SCADA Expert on the server, selecting Start Database will delete any previous database.

When you have created a blank database, you can proceed to set up the client connections.

For more information, see Welcome to the Client Administration Guide in the Geo SCADA Expert Guide to Client Administration.


Disclaimer

Geo SCADA Expert 2020