Geo SCADA Expert Performance Monitor Counters
The following table lists the Geo SCADA Expert Performance Monitor tags (see Access Property Tags) and the corresponding performance counters available in the Schneider Electric Geo SCADA Expert category of the Windows Performance Monitor.
There are four types of counters available in the Windows Performance Monitor:
- Elapsed—Use to measure the amount of computer processing time that is dedicated to an operation between samples.
- Sample Count—Use to show the number of events between samples. You can configure the sample period where the sample period can be configured in the Windows Performance Monitor tool.
- Total—Use to show the total number of events since the server was restarted.
- Current—Use to show the number of events that occur in real time (only used for logon counters).
The Geo SCADA Expert Performance Monitor tags provide corresponding functions to the Sample Count, Total and Current counter types.
| Geo SCADA Expert Performance Monitor Tags | Windows Performance Monitor Counters |
|---|---|
| Query Related Performance Counters | |
|
Query Execution (Elapsed) |
|
| QueryExecutePerSec |
Query Execution (Sample Count) |
|
QueryExecuteTotal |
Query Execution (Total) |
|
Query Parse (Elapsed) |
|
| QueryParsePerSec |
Query Parse (Sample Count) |
| QueryParseTotal |
Query Parse (Total) |
|
Query Verify (Elapsed) |
|
| QueryVerifyPerSec |
Query Verify (Sample Count) |
| QueryVerifyTotal |
Query Verify (Total) |
|
Query Optimize (Elapsed) |
|
| QueryOptimizePerSec |
Query Optimize (Sample Count) |
| QueryOptimizeTotal |
Query Optimize (Total) |
| Alarm Transition Counters | |
| AlarmTransitionPerSec |
Alarm Transition (Sample Count) |
| AlarmTransitionTotal |
Alarm Transition (Total) |
| AlarmRaisedPerSec |
Alarms Raised (Sample Count) |
| AlarmRaisedTotal |
Alarms Raised (Total) |
| AlarmClearedPerSec |
Alarms Cleared (Sample Count) |
| AlarmClearedTotal |
Alarms Cleared (Total) |
| AlarmAckPerSec |
Alarms Acknowledged (Sample Count) |
| AlarmAckTotal |
Alarms Acknowledged (Total) |
| AlarmRemovedPerSec |
Alarms Removed (Sample Count) |
| AlarmRemovedTotal |
Alarms Removed (Total) |
| AlarmRedirPerSec |
Alarms Redirected (Sample Count) |
| AlarmRedirTotal |
Alarms Redirected (Total) |
| Configuration Changes Counters | |
|
Config Changes Write (Elapsed) |
|
| ConfChngWritePerSec |
Config Changes Write (Sample Count) |
| ConfChngWriteTotal |
Config Changes Write (Total) |
| Events Processed Counters | |
|
Event Journal Write (Elapsed) |
|
| JournalWritePerSec |
Event Journal Write (Sample Count) |
| JournalWriteTotal |
Event Journal Write (Total) |
| EventsProcessedPerSec |
Events Processed (Sample Count) |
| EventsProcessedTotal |
Events Processed (Total) |
| Historic Write Counters | |
| Historic Write Annotation (Elapsed) | |
| HistWriteAnoPerSec | Historic Write Annotation (Sample Count) |
| HistWriteAnoTotal | Historic Write Annotation (Total) |
| Historic Write Modified (Elapsed) | |
| HistWriteModPerSec | Historic Write Modified (Sample Count) |
| HistWriteModTotal | Historic Write Modified (Total) |
| Historic Write Raw (Elapsed) | |
| HistWriteRawPerSec | Historic Write Raw (Sample Count) |
| HistWriteRawTotal | Historic Write Raw (Total) |
| Historic Write Suppression (Elapsed) | |
| HistWriteSupPerSec | Historic Write Suppression (Sample Count) |
| HistWriteSupTotal | Historic Write Suppression (Total) |
| Points Processed Counters | |
| AccHistoricPerSec | Accumulators Historic (Sample Count) |
| AccHistoricTotal | Accumulators Historic (Total) |
| AccProcPerSec | Accumulators Processed (Sample Count) |
| AccProcTotal | Accumulators Processed (Total) |
| Points CalcPoint (Elapsed) | |
| PointsCPntCalcPersSec | Points CalcPoint (Sample Count) |
| PointsCPntCalcTotal | Points CalcPoint (Total) |
| PointsEventsPerSec | Points Event (Sample Count) |
| PointsEventsTotal | Points Event (Total) |
| PointsHistoricPerSec | Points Historic (Sample Count) |
| PointsHistoricTotal | Points Historic (Total) |
| PointsProcessedPerSec | Points Processed (Sample Count) |
| PointsProcessedTotal | Points Processed (Total) |
| User Logon Counters | |
| UserLogon | User Logon (Current) |
| UserLogonViewX | User Logon ViewX (Current) |
| UserLogonWebX | User Logon WebX (Current) |