This section explains how to use the Service Manager. When you install Geo SCADA Expert on a server, you need to setup the Geo SCADA Expert server to run as a service so that you can start and stop the server when required. You may need to start, stop, and restart the Geo SCADA Expert server when you make changes to certain parts of the server configuration.
COMPLETE LOSS OF CONFIGURATION
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.