The WebX branch of the Server Status Tool includes a Clients category. The Clients category provides status information about each Original WebX client that is connected to the server.
                 
            
The status information for each Original WebX client is categorized under these headings:
- Address—The IP address of each client.
- Links—The number of links between the Original WebX client and the server.
- Up Time—The amount of time since the Original WebX client connected to the server.
- Licensed—Indicates whether the client has a valid license (Yes or No).
The number of clients varies according to the size of your system.
The Clients (WebX) category is often used to check that Original WebX clients have valid licenses (they will be unable to connect to the server if they have invalid licenses) and also to determine which Original WebX clients have a connection to the server.
Further Information