The WebX branch of the Server Status Tool includes a Cookies category. The Cookies category provides status information about each Original WebX cookie that is currently in use.
The server sends an Original WebX cookie to an Original WebX client when a user logs on via an Original WebX client. The cookie will remain valid as long as the Original WebX client is active within a 30-minute period. If the Original WebX client is idle for 30 minutes, the Original WebX cookie expires and the user will need to log on again as the cookie will be invalid.
                 
            
The status information for each Original WebX cookie is categorized as:
- Cookie—A Globally Unique Identifier (GUID) that is generated by the server to identify the cookie.
- User—The name of the User account that has been used to log on at the Original WebX client.
- Address—The IP address of the Original WebX client.
- Logons—The number of times the current User has simultaneously logged on to the Original WebX client. For example, if a user runs Internet Explorer and logs on to the Original WebX interface, then logs on again via a second Internet Explorer window, the Logons count will be 2 (the user is currently logged on via two browsers).
- Last Accessed—The time, in Coordinated Universal Time (UTC), at which the cookie was used to access the server. This time indicates when the user logged on to the Original WebX client.
Further Information