The Historic Searches category contains information about the searches that are currently requesting historic data. You can use the information to determine if a slow response to a historic data request is due to a large search or another factor such as abnormal network conditions.
                 
            
The Historic Searches category contains the following information:
- Id—A unique identifier for the search. This is used internally.
- Desc—A description of the function that is used for the search. This is used internally.
- Total—The number of historic records that have been searched and have data that matches the criteria set for the search.
- Time—The amount of time taken to process the search.
The ability to edit SQL queries that are used in query lists,