The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. The Server group provides status information about the server on which you are using the Server Status Tool and it contains the following sub-categories:
                 
            
- Advise Threads—Provides status information about the threads that are handling advise links.
- Advises—Provides status information about the advise links between the server and clients.
- Clients—Provides status information about each client that is connected to the server. The number of clients varies according to the size of your Geo SCADA Expert system.
- Comms Child Links—Provides status information about the connections that are multiplexed by the Comms Parent Links.
- Comms Parent Links—Provides status information about the connections between the server and clients.
- Comms Threads—Provides status information about the threads that are handling the server-client connections.
- Connected Workstations—Provides status information about each workstation that is connected to the server. A workstation is a client and is identified by its Workstation ID.
- Link Threads—Provides status information about the threads that are handling the server links.
- Privileges—Provides status information about server-wide user permissions.
- Server Links—Provides status information about the server links between the server and clients.