You can use the Information category to determine the status of the Database Web Server connection (see General System Status Information). The status for the connection between Geo SCADA Expert and the Original WebX displays the following two messages by default:
- Web Server: Running on Port <number>—The Database Web Server is setup correctly. Any web connection difficulties are likely to be related to your Internet connection or network settings.
- Secure Server: Running on Port <number>—The secure server is setup correctly. Any web connection difficulties are likely to be related to your Internet connection or network settings. However, you should also check that you have the correct Certificate and Private Key (see Original WebX Security Settings, Connection Settings and Preferences).
            The port Web Server port settings are also used by Virtual ViewX to display Mimics and Lists, (see Define the Ports Settings for Original WebX Clients). 
The following messages appear when a problem occurs relating to the Database Web Server:
- Port <number> already in use—The port is already in use by another internet application. You need to define a different port address for the web server or secure server (see Original WebX Security Settings, Connection Settings and Preferences).
- Web Server Disabled—Access via the non-secure port is not possible due to the web server being disabled (see Original WebX Security Settings, Connection Settings and Preferences).
- Secure Web Server Disabled—Access via the secure port is not possible due to the secure web server port being disabled (see Original WebX Security Settings, Connection Settings and Preferences).
- Failed to Create Socket—There is an error with the operating system network, please contact Schneider Electric for advice.
- Failed to Listen on Port <number>—There is an error with the operating system network, please contact Schneider Electric for advice.