Geo SCADA Expert installs files in several locations. Some of these files you may need to access during the configuration of your system and so you should familiarize yourself with the default locations.
The following sections detail the default file locations for Geo SCADA Expert on the following Windows platforms:
- Windows 64-Bit File Locations. This includes file locations for Geo SCADA Expert running on the 64-bit versions of Windows Server 2012, Windows Server 2012 R2, Windows Server 2016, Windows Server 2019, and Windows 8.1 and 10.
- Windows 32-Bit File Locations This includes file locations for Geo SCADA Expert running on the 32-bit versions of Windows 8.1 and 10.
These are the default file locations—the files on your system may be in different locations, depending on how the system has been installed and configured.
If you cannot locate a file at the default location, check the file's location using the Server Administration Tool, or use the Search facility in Windows.
You can change the location of the server files by using the Server Administration Tool. 
You can change the location of log files by using the Move Log Files wizard
Virtual ViewX
The following section details the default file locations for Virtual ViewX server on the following Windows platforms:
- Windows 64-bit File Locations – Virtual ViewX Server. This includes file locations for Virtual ViewX server running on the 64-bit versions of Windows Server 2012, Windows Server 2012 R2, Windows Server 2016, Windows Server 2019,  and Windows 10.(Virtual ViewX server is not supported on Windows 8.1.)