Geo SCADA Expert can be installed on 32-bit or 64-bit computers.
Systems running on server class hardware have to use 64-bit server operating systems such as Windows Server 2019, or Windows Server 2016. Server operating systems are designed for servicing entire systems rather than individual computers or small networks. For this reason, they are better suited for larger Geo SCADA Expert systems with more than two clients.
ATTENTION: Windows 8.1 and Windows 10 should not be used for servers with more than two clients. This is because the TCP/IP security measures in these operating systems can cause significant delays.
Small stand-alone client-server systems running on desktop class (rather than server class) hardware need to use operating systems that are appropriate to the computer hardware being used.
To provide database access from Geo SCADA Mobile, the servers have to run on server class hardware with 64-bit operating systems.
Likewise, to run Virtual ViewX, the Virtual ViewX server and Geo SCADA Expert server computers have to run on server class hardware with 64-bit operating systems (Virtual ViewX client computers can use 32- or 64-bit operating systems).
For more information, see Recommended Geo SCADA Expert Server Configurations.
Server class computers and virtual machines (VMs) on server class computers should not be used to run ViewX in a day-to-day operational environment; instead, appropriate client machines should be used. Client machines often have a higher graphics hardware specification than server class computers. This higher graphics specification is required to run ViewX in a day-to-day operational environment, within which users might perform graphics-intensive tasks such as viewing complex Mimics, or working with multiple or floating documents
The standard graphics hardware on server class computers and on VMs on server class computers may only be adequate for running ViewX for administrative purposes (such as performing initial system configuration and user account setup).