Geo SCADA Expert has a number of recommended operational limits. Expansion beyond the recommended limits is possible, but may result in a system that is unstable and unreliable. The recommended operational limits for Geo SCADA Expert clients are:
| Parameter | 32-Bit Limit | 64-Bit Limit | Notes | 
|---|---|---|---|
| Minimum ViewX to Geo SCADA Expert server link bandwidth | 2 Mbit | 2 Mbit | Exceeding these limits will cause slow performance in ViewX. | 
| Maximum ViewX to Geo SCADA Expert server link latency | 150 ms | 150 ms | Exceeding these limits will cause slow performance in ViewX. | 
| Minimum Virtual ViewX client to Virtual ViewX server link bandwidth | 1 Mbit | 1 Mbit | |
| Minimum Original WebX client to Geo SCADA Expert server link bandwidth | 2 Mbit | 2 Mbit | 
For information on server operational limitations, please see Operational Limitations - Server.