Trend Markers

Trend markers are indicators that represent the individual values of the source point. They are shown on traces and are displayed by default.

Trace Markers


If your User Account has the Configure permission, you can change the style and size of markers for each trace. You can choose from diamond, cross, or square shaped markers.

The color of the markers represents the quality of the data. The default marker colors are (from left to right):

Marker Colors

The marker colors for your system may be different to the above, as you can change the colors for each point by using the point’s Color Palette (see Configure the Display Settings for a Trend).

For data sources that are in the Geo SCADA Expert database, Geo SCADA Expert uses the appropriate color from the Color Palette (see System Colors). Again, the marker color varies, depending on the quality of the data, as described above. The applicable colors are prefixed with the word 'Trend' in the Color Palette, for example, Trend - Validated/Good Data. If Geo SCADA Expert is unable to obtain the marker color from the server (for example, if communications with the server is interrupted when a Trend is redrawn), Geo SCADA Expert will apply the marker colors that are defined in the Options window (see Define the Default Settings for New Trends).

Markers are shown on each trace by default, but you can choose to hide them as required (see Hide and Show Markers). The Hide Markers feature is often useful when there are multiple traces and the number of markers makes it difficult to use the Trend.


Disclaimer

Geo SCADA Expert 2020