Associated with: 'File' objects, such as Mimics, Reports, Trends, Logic programs, X-Y Plots, and X-Y-Z Plots
Security permission required to access this option: Read
Use the relevant Display option to display the selected ‘file’ object, such as a Mimic, Report, or Trend, in Run mode. (Run mode provides access to the 'file' object's operational features (as opposed to Design mode, which is the mode in which engineers configure the 'file' object).)
Depending on the part of the interface from where you select the Display option, the option name might also indicate the type of database item that will be displayed (for example, Display X-Y Plot). Both options perform the same function (they display the selected 'file' object in Run mode).