Locate in Database Explorer
This option is only available if:
- You are accessing an Object menu (other than from the Database Bar)
- Your user account provides access to the Database Bar.
Select the Locate in Database Explorer option for Geo SCADA Expert to display the Database Bar and highlight the item in the hierarchical ‘tree’ structure within that Explorer Bar.
Also see Locate in OPC Data Explorer.
You can also locate an item in the Database Bar by:
- Using the Locate command on the ViewX ribbon (see Display an Explorer Bar)
- Selecting the Locate in Database Explorer option from a document's tab (see Context-Sensitive Menu (Document Tab)).