You can rename any of the documents that are stored in your Operator Document Store(s). This is useful when a document has been provided with a misleading name or there is a mistake in the name.
To rename a document in your Operator Document Store:
- Log on to ViewX.
- Display your Operator Document Stores (see Access Your Operator Document Stores).
- Expand your Operator Document Stores until you locate the document that you want to rename.
- Right-click on the document, then select the Rename option from the context sensitive menu.
 The document is selected automatically, ready for you to define its name.
- Overwrite or amend the existing name as required, then press the Enter key or select another part of the interface to confirm your entry.