Which Type of Client Should I Use?

We recommend that you use ViewX clients for day-to-day and long-term use in Control rooms. ViewX is the client that also provides administrator- and configuration-level access to Geo SCADA Expert (for User Accounts that are configured to provide such levels of access). Virtual ViewX and Original WebX only provide operator-level access to the database (once you have logged on with a valid Geo SCADA Expert User Account).

Virtual ViewX clients are web-based clients that are intended to provide occasional, operator-level, remote access to the database. The benefits of Virtual ViewX clients compared to ViewX clients include:

The benefits of ViewX clients compared to Virtual ViewX clients include:

Additionally, ViewX clients can provide the following functionality:

(Original WebX is the deprecated web client that is supported by this and previous versions of Geo SCADA Expert. Your system might use Original WebX clients if it has been upgraded from an earlier version of the product. For more information about this type of client, see Original WebX Client.)


Disclaimer

Geo SCADA Expert 2020