Configure Most Settings using Geo SCADA Expert
            If you want to use Geo SCADA Expert to configure most or all of the incremental configuration settings, you can use the following strategies:
- Minimum Configuration in Configuration Application, Load Into Field Device, Upload to Geo SCADA Expert
 - Minimum Configuration in Configuration Application, Import into Geo SCADA Expert, Download to Field Device
 - Minimum Configuration in Configuration Application, Load into Field Device, Import Into Geo SCADA Expert, Download Changes