Database Items Required for WITS

For Geo SCADA Expert to be able to communicate with a WITS Field Device, it needs to have these items configured in the database:

For the initial configuration, you do not need to create database points (unless you are using Group Templates, see Using Group Templates with WITS Field Devices). Geo SCADA Expert creates these automatically when the Field Device's configuration is imported or uploaded. Geo SCADA Expert also creates items for time profiles automatically, and if you upload the configuration, it also creates application program items.

Each of the database items listed above needs to have certain 'minimum' configuration settings in place.These vary depending on the type of Field Device and communications. When you are configuring these items, any invalid or required configuration is indicated by a message shown at the bottom of each configuration Form.

When the Device Profile, Channel(s), Outstation Set, and Outstation items are configured correctly, the Field Device's bulk configuration and matching incremental configuration files can be imported/uploaded into Geo SCADA Expert.

Geo SCADA Expert uses the incremental configuration file to create items for WITS points and profiles automatically. (Geo SCADA Expert is also able to create Application Program items automatically, but only if the configuration is uploaded). The WITS items that Geo SCADA Expert creates match the inputs, outputs, and profiles used by the Field Device, as specified in the incremental configuration file.

If required, you can create additional time profiles and application programs in Geo SCADA Expert and then download them to your Field Device. This is dependent on your Field Device supporting configuration download, and each Field Device supports a limited number of profiles and applications (defined in the Device Profile, (see WITS Device Profiles)

Further Information

WITS Device Profiles

Configuring a WITS Device Profile

WITS Bulk Configuration Files, Incremental Configuration Files, and Application Program Files

DNP3 Channels: see Configuring a DNP3 Channel.

DNP3 Outstation Sets: see Configuring a DNP3 Outstation Set.

WITS Outstations: see Configuring a WITS Outstation


Disclaimer

Geo SCADA Expert 2020