General Point Properties - WITS Runtime Points
Use the fields at the top of the Runtime tab to specify the General Properties of a DNP3 Counter Point
The following field is specific to the WITS driver:
- Point Number—Enter the number that represents the virtual counter point that will store the runtime value. Geo SCADA Expert cannot perform any validation on the number you enter. If the number you enter does not represent a valid counter point, then any configuration download to the device will not succeed. For more information, see the Field Device documentation.