Override

Associated with: WITS Points (that support the Override feature and have it enabled).

Security permission required to access this pick action: Override/Release.

You use the Override action to temporarily override a point's measured value with a new value.

You can apply an override to a point in both Geo SCADA Expert and/or the Field Device. A Geo SCADA Expert override does not affect the value of the point in the Field Device. An override in the Field Device is called an 'Outstation Override' in Geo SCADA Expert.

To return to using the measured point value, you use the Release Override action.

You might use the Override action:

Using the Override action can help to prevent Geo SCADA Expert or the Field Device from raising alarms unnecessarily, and can help to ensure that accumulators remain accurate.

The device profile indicates the types of point (if any) you can override in the Field Device. You can override all types of point in Geo SCADA Expert (see Display a WITS Device Profile).

To enable the override feature, you use the fields within the Point Form's <Point Type> tab (see Define whether an Analog Point can be Overridden and see Define whether a Digital Point can be Overridden and see Define Whether a Counter Type Point can be Overridden).

To apply an override to a point's value, follow this procedure:

  1. Select the Override action to display the Override window.

  2. In the Location field, use the combo box to specify the override location. You can override the point in Geo SCADA Expert (the Master Station) or in the Field Device (the Outstation).

    A derived point in the Field Device will also use any override applied to its parent point in the Field Device.

  3. For analog points and counter points: In the Value field, specify the override value. Enter a value within the range specified by the user when enabling the override feature for the point. Geo SCADA Expert displays a message if you enter a value outside this range.

    For digital points: Use the combo box to specify the state to which you want to override the point.

  4. Select the OK button to apply the override. Depending on the system configuration, Geo SCADA Expert may prompt you to confirm your override request.

    When you remove an override from an analog input point in the Field Device, the Field Device applies any configured hysteresis or persistence to the point if the point may subsequently move from one state to another (including the normal state). Similarly, when you remove an override from a binary input point in the Field Device, the Field Device applies any configured persistence.

Whenever Geo SCADA Expert overrides a point's value:

A Field Device may allow you to apply and release overrides locally (in addition to applying them from Geo SCADA Expert). The Field Device sets the DNP3 object status flag 'local forced' while the point is overridden. Geo SCADA Expert shows this status in the relevant displays.

A configuration upload includes any overrides a user has applied or released locally at the Field Device ((see Upload Configuration (WITS Outstation))).

Further Information

Actions that are Common to Many Drivers.


Disclaimer

Geo SCADA Expert 2020